7/17/2022 12:10 PM | |
Joined: 6/25/2022 Last visit: 7/20/2022 Posts: 4 Rating: (0) |
Hello, I'm currently using a 6ED1052-1MD08-0BA1 and put an 8Go MicroSD card formatted in FAT32 into it. I want to record two analogical mementos, however, the records are staying put in the logo ROM and won't go into the SD card. I don't know how to resolve it, because it worked before. Here is the archive of variables : thank you in advance AttachmentNouveau dossier.zip (328 Downloads) |
Last edited by: Lapin25 at: 07/17/2022 13:36:50 |
|
7/17/2022 1:09 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32887 Rating: (4066)
|
Please can you upload your program as a ZIP file? |
7/17/2022 4:28 PM | |
Joined: 6/25/2022 Last visit: 7/20/2022 Posts: 4 Rating: (0) |
here is my program
AttachmentNouveau dossier.zip (284 Downloads) |
7/17/2022 4:58 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32887 Rating: (4066)
|
I upload your program to my LOGO! and start the LOGO!. It would created a Data Log and I can it download. What is exactly the problem? No Data Log? If yes, then have a problem with your SD card. Or Data Log with wrong data? And you have a overlapping in your Parameter VM Mapping list. The address is the start address of the byte address. A VW is a word and has two bytes. VW1 = VB1 and VB2. Both words write in VB2. Edit: Attachment192.168.178.33 _ -1_2022-7-17 16-48-49.zip (275 Downloads) |
Last edited by: ixo65 at: 07/17/2022 17:00:52 |
|
7/18/2022 12:47 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32887 Rating: (4066)
|
I don't know if it is possible to make a Data Log and using Access Tool at same time. I never try it. For this case start a Support Request. |
This contribution was helpful to1 thankful Users |
7/21/2022 7:22 AM | |
Joined: 9/11/2014 Last visit: 4/26/2024 Posts: 716 Rating: (27) |
Hi, did you try a MSD-Cards from another vendor? |
Follow us on