2/23/2021 4:49 AM | |
Joined: 5/24/2018 Last visit: 2/7/2023 Posts: 26 Rating: (0) |
Good morning dear friends, I am trying to communicate an hmi ktp900 with the abb dcs through a modbus master tcp / ip, since the hmi also supports this protocol, and seeing that with allen braledy it is possible through ethernet ip, then and trying to execute similar procedure but when selecting the modbus tcp protocol I can't put the IP of the modbus master, I see another driver called mitsubishi mc tcp / ip here if it gives me the option to put the IP of the plc, but no I don't know link if I will succeed do it this way. The question is that you can make this connection by modbus TCP / ip with the master ci867, someone has done it, and if so, what would be the procedure or what do you need? Greetings
Attachmentimagenes.pdf (125 Downloads) |
2/23/2021 8:48 AM | |
Joined: 6/19/2017 Last visit: 6/5/2024 Posts: 8147 Rating: (165) |
Closed cause question posted twice. The second thread with the subject KTP900 modbus tcp with ci867 modbus master is published within the conference Communication / Networks. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on