5/27/2021 9:32 PM | |
Joined: 6/20/2010 Last visit: 10/6/2024 Posts: 96 Rating: (0) |
Hi, I just have similar problem, my clock inside work well when simulate, but inside LOGO 8.3 new when activate the output after the time off the output keeps ON. I use seven UDF and only it happens in one of them. I create a different UDF with different name and the same problem. I changed the output and I have two problems now I`m thinking change LOGO, but it`s new Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/28/2021 08:41:30New subject after splitting |
|
5/27/2021 9:40 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
A screenshot of apart of the UDF is not helpful. Please upload the UDF if you want help. |
5/27/2021 10:39 PM | |
Joined: 6/20/2010 Last visit: 10/6/2024 Posts: 96 Rating: (0) |
Ok I will send tomorrow, I'm working now all night. Thanks. |
5/28/2021 8:05 AM | |
Joined: 6/20/2010 Last visit: 10/6/2024 Posts: 96 Rating: (0) |
Good morning Ixo, you can download from here. But I do not see which is the problem. [snip] AttachmentUDF_CARAZO7.zip (382 Downloads) |
Last edited by: Jen_Moderator at: 05/28/2021 08:44:12Removed link and added file as an attachment. |
|
5/28/2021 9:07 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
I think you should have Siemens check your UDF and your LSC diagram where the UDFs are called. To do this, start a Support Request.
|
5/29/2021 12:45 PM | |
Joined: 6/20/2010 Last visit: 10/6/2024 Posts: 96 Rating: (0) |
OK Ixo, I´ll make it. Thanks |
6/6/2021 2:07 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
That's a knowed problem. But you upload only the UDF to the forum without the program. So we don't see it. |
Follow us on