11/5/2020 9:39 AM | |
Joined: 7/5/2017 Last visit: 6/16/2024 Posts: 10 Rating: (0) |
Hello. I have some trouble with connectiong Logo!8 and CPU 315 2xDP with CP343-1 Lean. communication. Anyone know if this is possible? I can not choose S7 connection from my PE/IE, and on the 315, when make a new connection, I can not choose the PE/IE. Only UDP and TCP connection. Is ii possible to make connection between Logo and 315 cpu with TCP or UDP? I will attach some screenshoots of my communications. All answers are much appreciated, cheers!! Attachment315 CPU.zip (284 Downloads) |
Follow us on