4/18/2017 4:05 AM | |
Joined: 2/24/2017 Last visit: 12/9/2022 Posts: 33 Rating: (1) |
hello I need to some beginner and intermediate examples for LOGO 8 Master/Slave |
4/18/2017 7:30 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
In attachment a simple example for LOGO! 0BA8.Standard master-/slave-communication. You must set the slave LOGO! especially in slave mode. Tools > Transfer > Configure Master / Slave Mode AttachmentLOGO! 0BA8.Standard_Master_Slave_communication.zip (2102 Downloads) |
This contribution was helpful to2 thankful Users |
4/23/2017 10:05 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
I have the above example still to the reading of analog inputs of the slave LOGO! and writing to analog outputs of the slave LOGO! expanded.
AttachmentLOGO! 0BA8.Standard_Master_Slave_communication_V2.zip (1043 Downloads) |
This contribution was helpful to1 thankful Users |
4/24/2017 9:12 AM | |
Posts: 153 Rating: (16) |
LOGO!8 – Simply ingenious. Simply more. |
This contribution was helpful to1 thankful Users |
Follow us on