11/10/2008 1:43 PM | |
Joined: 3/14/2008 Last visit: 8/30/2024 Posts: 2093 Rating:
|
Hello, I have a question regarding the LOGO plc basic version. In a project, the logo is used but for automation, the logo is too small. I was wondering if the logo could be used as a slave and if the master can be a s300 plc. Or can the logo be used only with expandable modules?. Thank you Grtzz Sandor |
If I could help you, you can use the RATE button. Thank you. |
|
11/10/2008 2:28 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hi LOGO works like slave on S7-200 PLC master. More about this read in FAQ: What devices do you require to operate LOGO! modules on the AS-interface bus, and in which form is data exchange possible? regards |
Follow us on