7/22/2022 2:01 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello behnam ba, FC is the function, example FC2405. There are some reasons if the download to the CPU ist not possible:
I recommend to make the check block consistency. See also the information of the FAQ: How do you perform a block-consistency check following changes in the STEP 7 program? Check also the PG/PC interface and see the remedy in the FAQ: How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible? With best regards |
Follow us on