8/2/2022 11:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please visit https://www.sow.siemens.com/ page & enter desired article number of which spares you want, click search & detail applicable spares list will be displayed. You can export the displayed spare list in EXCEL format also. (refer attachment) Hope this helps. AttachmentS120 MM spares list.zip (313 Downloads) |
8/3/2022 8:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello INDRA, Since it is successor product, no much parameters needs to be modify. Please check what topology sensitivity is set in p9906. Please refer Replacement of S120 componenets topic which will help you to understand P9906 setting. If it high i.e. 0, you need to set it 2 i.e. low type & then change Motor module. or else you can set p9909 value (explained in same post) so that new motor modules serial numbers & hardware versions are automatically transferred to CU. Remember these values are saved in RAM which you need to save in ROM permanently by p0977 to 1. Hope this helps. |
8/3/2022 2:31 PM | |
Joined: 3/10/2022 Last visit: 8/4/2022 Posts: 16 Rating: (0) |
Hi Piscean, Thanks again for your info. I'll try it when my order new successor arrived in mill regards indra |
Follow us on