6/2/2014 1:25 AM | |
Joined: 9/27/2006 Last visit: 9/13/2025 Posts: 12408 Rating:
|
Hello Negro; Have a look at this comment from member nhdrives, from a similar thread (in 2008): To control a Masterdrives via DeviceNet, you need the CBD (CommBoardDevicenet) in the drive. The functionality of the CBD is described in its eds-file (electonic data sheet). If you do not have the CBD (6SX7010-0FK00), look here for information: Communiation board CBD DeviceNet - Industry Mall If you do not have DriveMonitor, have a look at this update: The part number for the DriveMonitor CD is shown in that link. Meanwhile the EDS file for the Masterdrive CBD is available on the web here (as a text file): http://manuali.eltex.biz/Manuali_Siemens/Inverter/Simovert/Options/CBD.eds Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/2/2014 2:09 AM |
|
This contribution was helpful to
1 thankful Users |
12/19/2024 8:33 PM | |
Joined: 1/22/2008 Last visit: 7/30/2025 Posts: 1 Rating:
|
Hi, I've seen this answer regarding the EDS files but unfortunately the link that you mention is not available. Do you have any idea where I can find it? Many thanks, Beatriz |
12/20/2024 8:32 AM | |
Joined: 3/25/2008 Last visit: 9/11/2025 Posts: 224 Rating:
|
manual
Attachmentop_cbd_e.pdf (293 Downloads) |
12/20/2024 8:35 AM | |
Joined: 3/25/2008 Last visit: 9/11/2025 Posts: 224 Rating:
|
CANOpenEDSFiles
AttachmentCANOpenEDSFiles.zip (210 Downloads) |
Follow us on