5/24/2024 3:58 PM | |
Joined: 3/30/2020 Last visit: 6/25/2024 Posts: 21 Rating:
|
Hi, I am Baldeep Singh and i am using Siwarex WP251 with PLC S7 1200 CPU 1215C DC/DC/DC and i am having issue with the max correction action. I know that max correction action is the( percentage x Target Weight) and it will correct the next trailing weight to get close to the Target Weight. My configuration is Target Weight = 250 KG Tolerance = (+ -)500g Fine Weight is 35KG Trailing weight = 5KG Proportional controller activated. But i keep getting Over 250 kg and the max correction action seems to be not working. I want to know whether there is another parameter i need to set and is my understanding for this proportional controller is correct. I have also attached my siwatool file here. Thanks, Baldeep Singh AttachmentSiwatool_FIBC.zip (67 Downloads) |
Last edited by: AutoGen_6958441 at: 05/25/2024 02:47:41 |
|
5/31/2024 12:07 PM | |
Joined: 1/4/2007 Last visit: 7/11/2024 Posts: 1134 Rating:
|
Hello Baldeep, Please take a look to the attached file. Best regards Siwarexi
|
Follow us on