2/25/2013 11:36 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Hello, I configured WinCC AlarmControl on the server. It displays Date, Time, Status, Alarmtext in runtime (headers). However, on the Client the names are different: Logging, Comments, Computer name, Process value 5...How can i change the names on the client? Server data is loaded succesfully |
If I could help you, you can use the RATE button. Thank you. |
|
2/25/2013 11:55 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Little bit to fast post: Text library needs to be the same as for server... When is this done automatically? Or do you have to do this manually? |
If I could help you, you can use the RATE button. Thank you. |
|
2/28/2013 1:03 PM | |
Posts: 1530 Rating: (59)
|
Hello Oreca, if I take a look at manual of Client-Server, Chapter 3.7 and 5.7 I'd say it should work and actualization should be done automatically if Server-Client-Connection if working fine. Best regards Bizur |
3/1/2013 8:27 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
I think there is something wrong with the setup of those client server systems.... The ES used to be a OS, graphics designer cannot be opened on ES, only on server... So I think I'm gonna blame the setup then.... I will look at the manual, thx for suggestion |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on