4/24/2016 9:16 PM | |
Joined: 5/28/2008 Last visit: 5/26/2024 Posts: 4506 Rating: (836)
|
Hello, As friends told here, check the Set point sent via telegram and Control Word as well. I recommend to use the FC14 as per the link bellow to control MM$ via profibus. Please feedback us if there are any other problems. MICROMASTER 4 & SINAMICS G120: Function block (FC14) to control an MM4 via PROFIBUS DP |
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
5/3/2016 9:34 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by SaeedRadin is split to a separate thread with the subject How i can run MM420 with S7-414 with profibus?. Best regards |
This contribution was helpful to1 thankful Users |
Follow us on