7/4/2007 10:43 AM | |
Posts: 1 Rating: (0) |
Hallo, die Firma Balogh aus Frankreich bietet eine Profibus-Anschaltung für das Moby-M System an. Mit freundlichen Grüßen http://www.balogh-rfid.com |
7/7/2007 12:01 PM | |
Posts: 2 Rating: (1) |
Hello Xavi, I had the same problem as you! I also try the module from Balogh, but it's not fully compatible with MOBY-M devices, there are problems with writing or readind data from tags. But I can recomend you an another device, the name is ZITA1206. It's a small gateway, that alowes you to connect your S7300/400 PLC to MOBY-M head (LBS) over PROFIBUS DP or ETHERNET. The module include a Step7 library, that willhelp youeasyly integrate itto your control system. The company name is CIM SLOVAKIA, just try this email cim@cim.sk bye AttachmentZITA1206.pdf (814 Downloads) |
Last edited by: AngelG at: 07.07.2007 12:42Last edited by: AngelG at: 07.07.2007 12:38 |
|
7/17/2007 4:51 PM | |
Posts: 9 Rating: (0) |
Thank you very much. |
Follow us on