3/30/2016 6:38 PM | |
Posts: 63 Rating: (1) |
Hi folks, I am using Done and Error as condition to call the next Mudbus_master. After a while the communication stopped because one of the Modbus_masters got stuck on Busy. Does anyone know why this is happening? According to someone I talked to at the SIEMENS Support then this is not supposed to happen. The Blocked_Proc_Timeout is supposed to prevent this. This Blocked_Proc_Timeout is set default to 0.5 (I am guessing that is seconds.) How does this differ from the RESP_TO that you set in the Modbus_Comm_load? Because that is set default to 1000 (1s). In attachment (Download from WeTransfer) is a project where I am shifting between two devises. In NW3 I added a condition that if MB_master is busy for more 1s then it goes to next device. This seems to work but I don’t want to have it if there is a better way. Perhaps someone can send me a project they have done with multiple master block that works.
Attachment: http://we.tl/drp46an9W0 |
4/15/2016 12:14 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating: (12) |
Hi, Can you attach the program once again? It has expired. |
4/16/2016 5:22 AM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308)
|
I had faced a similar problem ( Busy bit gets stuck ). The TImer output is used reset and re-trigger communications. |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
4/16/2016 10:56 AM | |
Posts: 63 Rating: (1) |
Hi, O, Sorry her is a new link from my Dropbox. That wound expire. Is folder MB_Busy_to_long. https://www.dropbox.com/sh/wtkwd912950mlfo/AAAXXNAtuyxidVHF_KmFA9uUa?dl=0 Regards HannAri |
4/18/2016 2:04 PM | |
Posts: 63 Rating: (1) |
Hi Navnag. How do you go by reseting and re-triggering the communication? |
6/8/2016 8:53 AM | |
Joined: 8/21/2014 Last visit: 10/8/2024 Posts: 1024 Rating: (14) |
New question published by andersonpss is split to a separate thread with the subject How to reset Modbus_Master in the ET200SP. Best regards |
My Forum is the place to personalize your profile, |
|
6/27/2016 4:57 PM | |
Posts: 63 Rating: (1) |
Hi again. What do you mean by this? |
Follow us on