5/31/2016 4:02 AM | |
Joined: 2/6/2009 Last visit: 6/18/2024 Posts: 939 Rating: (118) |
Dear All, Attached is the sample project for the Modbus communication between ET200SP CM PtP - 6ES7 137-6AA00-0BA0 and the third party (slave) devices.Manual for slave devices used in program backup also integrated in the attachment. Main driver block is FB50 (Modbus_Master_SCL) and this block should be called for each CM PtP module. Blocks associated with the FB50 is, Modbus Comm Load Standard FB Modbus_Master Standard FB FC 50 = Block_Move DB150 = Send list DB (Modbus Queries list) DB151 = Modbus Data (Received Data’s) Advantages of using this block,
Use the Modbus block and achieve communication tasks quickly and easily without any problem. Please revert back for any clarification AttachmentCM Ptp Modbus Master V1.0.zip (2322 Downloads) |
Last edited by: Saravana kumar at: 12/6/2016 6:32:06 AMLast edited by: Saravana kumar at: 12/6/2016 6:32:28 AM_______________________________________________________________ |
|
This contribution was helpful to1 thankful Users |
5/31/2016 4:09 AM | |
Joined: 2/6/2009 Last visit: 6/18/2024 Posts: 939 Rating: (118) |
Hi All, Please find the attachment for the Part 2 of the CM Ptp Modbus Master V1.0.zip file. Change the file name as 'CM Ptp Modbus Master V1.0.z01' before extracting the files. AttachmentCM Ptp Modbus Master V1.0 - Part 2.zip (1511 Downloads) |
_______________________________________________________________ |
|
6/22/2016 2:47 PM | |
Joined: 12/7/2010 Last visit: 6/28/2024 Posts: 89 Rating: (0) |
Not Able to open project after downloaded two zip file. procedure done as per your direction. |
10/27/2020 1:18 PM | |
Posts: 3 Rating: (0) |
Hi Saravanan , i can not extract even after renamed , is there any other way to open it ? |
5/6/2021 9:11 AM | |
Posts: 1 Rating: (0) |
Dear Saravana Kumar. Do you have project with modbus write function? Thanks. |
Follow us on