11/8/2023 6:47 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, is really easy to find similar Topics (exactly explained by me f.ex.) on Forum where this problematic is described and explained, mostly to exact problem of user situation. Look inside this Conference a few Topics bellow yours: Read Coils and Inputs with Modbus protocol Hope you understand that this problematic isn't easy to describe on one page. Generally help in TIA is enough to understand how this system is working. Becxause Modbus is standard, you can also check general problematic with Modbus RTU data accessing, also inside TIA help about RTU blocks where registers are described and what memory and areas they occupy. Just one example and logical tip. To understand Modbus system, Holding register can be defined with WORD data type as general access so it is typical one register length. How to access then REAL value in this memory? Easy and logical if you think how many WORDs use REAL data type, then LEN parameter can define how much WORDs you want read/write. This also explains that REAL value is nothing else than 2 WORDs value inside your Holding register at specific offset |
Last edited by: Duris_I at: 11/08/2023 06:51:55Last edited by: Duris_I at: 11/08/2023 07:48:41Last edited by: Duris_I at: 11/08/2023 08:01:41With best regards... |
|
Follow us on