7/27/2018 1:15 PM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
Hi Yu-Wen Teng, I am using the cpu 6ES7 515-2AM00-0AB0. I have followed all steps as per your document. When I compile my program. There are few data type errors like TCON_IP_v4_SEC. I have attached the project for referance. Thank you. Regards Satheesh
Application Example for SIMATIC S7-1500 V1.0.zip(154 Downloads) ------------------------------------------------------------------------------------------ AttachmentMQTT SERVER_1_20180727_1913.zip (286 Downloads) |
Last edited by: Jen_Moderator at: 7/30/2018 9:30:27 AMNew subject after splitting and inserted quotation. Thanks |
|
7/30/2018 10:14 AM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Dear Satheesh, As mentioned in my document, for the reason of supporting the secured communication, you need a S7-1500 CPU with V2.0 or higher. You have a project with CPU V1.8, that's why you got "TCON_IP_v4_SEC" compiled errors. I have modified your project making it fit for V1.8 (secured communication not supported). The project is compiled without error. Best regards, Yu-wen AttachmentMQTT SERVER_1_20180727_1913_1.zip (347 Downloads) |
This contribution was helpful to1 thankful Users |
7/31/2018 2:57 PM | |
Posts: 1368 Rating: (126) |
Hello, you can use the test broker from mosquito to publish messages. Here you find the description of the test-broker But please note: Please don't publish anything sensitive, anybody could be listening! In SIOS, you also find a program for MQTT Here, you find a solution for secure communication and unsecure (S7-1500 FW <2.0 or S7-300) |
This contribution was helpful to2 thankful Users |
7/31/2018 5:07 PM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Thanks a lot to Pittiplatsch for the answer. Dear Satheesh, |
This contribution was helpful to2 thankful Users |
8/1/2018 3:29 PM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Dear Satheesh,
Best regards, Yu-wen |
This contribution was helpful to1 thankful Users |
Follow us on