10/30/2018 1:53 PM | |
Joined: 5/6/2010 Last visit: 10/12/2024 Posts: 1984 Rating: (278) |
Hi MFMF, that sounds good that I'm understanding your challenge. I attached a project, created with TIA V14 SP1, written in FUP for easier understanding. The program start the LED chain with the "FirstScan"-flag and set (with a constant time difference) LED by LED . Hope this is helpful. If you have any questions.. don't hesitate regards AttachmentTest_LED_20181030_1413.zip (171 Downloads) |
Last edited by: CaOd at: 10/30/2018 2:18:20 PM |
|
11/1/2018 10:32 AM | |
Posts: 15 Rating: (0) |
Hi CaOd and everyone else, I have changed the CPU and Signal Module and put it under TIA compressed file. CPU : 1512SP F-1 PN The objective has still not been met (Signal Module to automatically switched on its LED 1 to LED 8 when PLC is switched on). The file that I have shows minimal warnings and no error. The warning that was seen after some edit would be error in lower-level component which is easily solved by Assigning address (The yellow circle with red dot) and upload into device. AttachmentAttempt.zip (153 Downloads) |
11/2/2018 7:38 PM | |
Joined: 5/6/2010 Last visit: 10/12/2024 Posts: 1984 Rating: (278) |
Hello MFMF, I will check your project during the weekend. regards |
Follow us on