1/28/2020 7:39 AM | |
Joined: 5/18/2015 Last visit: 11/9/2020 Posts: 67 Rating: (2) |
Hi All, I need to convert proTool project from MP270B 10" KEY panel 6AV6 542-0AG10-0AX0 to only available replacement now: KP1200 Comfort 6AV2124-1MC01-0AX0. So ProTool -> TIA with WinCC SP2. My PG came up with WinCC SP3. Linked SP2 requires preinstalled lower versions: "The Download of the service pack 2 requires an installed WinCC flexible 2008 or WinCC flexible 2008 SP1". I can only find installation download for SP3 and SP5.. is there SP1 or SP2 full version installation anywhere? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/28/2020 12:17:48New subject after splitting |
|
Follow us on