7/30/2022 9:46 PM | |
Joined: 4/5/2022 Last visit: 7/31/2023 Posts: 3 Rating: (0) |
Hi sir's... Please suggest as soon as possible... In master drive VC CU2 v1.3 After change from P163-4 with encoder to P163- 1 V/F mode without encoder, to check encoder problem or not, after check while normalise to P163-4 then parameters start reseting automatically. After that I set P51-3 and P52-5 to change parameters but not accepting any parameters to change, even change from P52- 5 to P52-0 also not accept (in PMU shows - - - - after pressing P to change value). Please suggest I need to download backup program Waiting for yours precious response URGENT.... Thanks and regards ------------------------------------------------------------------------------------------ |
Last edited by: Budan at: 07/30/2022 21:50:04Last edited by: Jen_Moderator at: 08/01/2022 10:45:02New subject after splitting |
|
Follow us on