5/20/2014 2:48 PM | |
Joined: 1/16/2012 Last visit: 9/8/2022 Posts: 72 Rating: (3) |
I'm using v5.5 + SP3. MLFB is part of the Part number? I cannot see any of them in the HW config, see attached. |
5/22/2014 8:08 AM | |
Posts: 559 Rating: (87) |
You need to upload the backup from individual IM CPU. Add into the same project & Then again upload the backup from the Main CPU. Try it out. |
5/22/2014 9:04 AM | |
Joined: 1/16/2012 Last visit: 9/8/2022 Posts: 72 Rating: (3) |
You can't see much in it, just the main CPU. |
Follow us on