1/19/2024 1:17 PM | |
Joined: 3/4/2020 Last visit: 4/25/2024 Posts: 29 Rating: (0) |
We changed the CPU card of a 840D NCU572.5 for a new one because it was having big problems with random communication fails. It's commanded with an IPC with Windows XP, HMI Advanced 7.06.02.02 and a customized interface, based on Visual. It has been working since 2016 with this configuration and we only changed the CPU card and loaded the arc backup files and everything looks working fine, except the OEM warning messages from PLC (700000 warnings ) that doesn't appear with text (just number). If I try HMI Startup the problem is the same: PLC warnings with no message. All warning text files, with different languages, are inside the proper folders of the HMI Advanced as you can see on the pictures attached. The warnings are just working alarms, like "emergency pressed", "barrier disabled"... I have been following the HMI Advance Operator's Manual and everything looks ok. Actually we didn't change the IPC setup. Any idea? AttachmentWarnings No Text HMI STARTUP.zip (105 Downloads) |
Last edited by: Boskyman at: 01/19/2024 13:19:10Last edited by: Boskyman at: 01/19/2024 14:43:53Living between Spindles, Waterjet heads and Lasers... |
|
Follow us on