2/24/2021 12:09 PM | |
Joined: 6/20/2020 Last visit: 4/4/2024 Posts: 42 Rating: (0) |
Hello, I don't know if the problem come from the LWE 1.1.0 or if i make a mistake but i am not able to read value of an hour counter (VD) on the Webserver when the value exceed 65535. When OT value is 1092h (65520m), it's OK, but when it's 1093h (65580) the result is "unsupported." I don't know why because it's not a VW but a VD. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/24/2021 14:02:17New subject after splitting |
|
2/24/2021 1:17 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33165 Rating: (4098)
|
Please upload the LWE project and the LOGO! program as a zip file. |
2/24/2021 2:41 PM | |
Joined: 6/20/2020 Last visit: 4/4/2024 Posts: 42 Rating: (0) |
That's what I thought. thanks for trying yourself. |
This contribution was helpful to1 thankful Users |
10/18/2021 1:50 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33165 Rating: (4098)
|
No, there is no other solution. Siemens has to fix the bug in LWE. |
10/19/2021 10:21 AM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33165 Rating: (4098)
|
I don't know, I'm not Siemens. Only Siemens can give you a answer ... |
Follow us on