2/8/2023 2:32 PM | |
Joined: 6/28/2022 Last visit: 4/18/2024 Posts: 27 Rating: (0) |
I have no idea what is wrong so im going to provide as many details as possible, cause i dont know where the fault is.
I have set up my devices within TIA as they are in real life (see image). The slave device was added through a gsd file. I gave the slave device profibuss address 4, i also set the software in the inverter to be on adress 4 for profibus. To thedevice overviewfor the slave device i added Standard telegram 1 .I usedDownload to Devicefor both hardware and software, successfully. I then click Go online. However, modules/devices are marked with Errors or Not reachable. In the diagnostics window for the PLC get this message (IO Device failure): "The IO device specified in the detailed information has failed or is not present. Check whether the failure belongs to an intended maintenance intervention. Check whether the failure occurs once or is repeatedly coming/going. Check whether there are more device failures and locate the failed device(s) in the IOSystem topology. Regard special device types (e.g. I devices, IE-IE-IOC) Remedy: Check power supply, network wiring and connectors." I don't know if any more information is required. But i have attached a few images in the rar (its a rar, i just changed name of the file extension since i could not upload rar). AttachmentNotReachable.zip (291 Downloads) |
Last edited by: KevinNfoDrives at: 02/08/2023 14:33:55Last edited by: KevinNfoDrives at: 02/08/2023 14:34:39 |
|
Follow us on