8/27/2021 6:19 AM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33413 Rating:
|
Operating Manual LOGO! CIM Edition 10/2021 LOGO! CIM provides Internet connection solution for LOGO! BM, S7-200 SMART CPU and SMART LINE which have more and more capabilities to interact with Internet now. General introduction Universal Data Model (UDM) LOGO! BM, S7-200 SMART CPU, SMART LINE, and Modbus RTU compatible devices can map their process data to UDM. UDM acts as a data center for LOGO! CIM, and different protocols can exchange data through UDM. 4 ports switch CIM can work as a LAN switch. To ensure CIM work stably and efficiently, Siemens recommends that you should connect less than 10 devices to CIM through Ethernet switch ports. General gateway LOGO! CIM can access the Internet with cellular module and SIM card installed. LOGO! BM, S7-200 SMART CPU, SMART LINE, or Modbus RTU compatible devices can access the internet by connecting to LOGO! CIM. Further functions The CIM supports the following functions: • Web-based configuration A Web-based user interface (Web-based configuration) for the configuration of the CIM. • Protocol gateway LOGO! BM, S7-200 SMART CPU, SMART LINE and Modbus RTU compatible devices can communicate with LOGO! CIM via S7/Modbus protocol based on the Universal Data Model (UDM). Application can access data through RESTful API on LOGO! CIM based on UDM. • Data management CIM can perform an action when a configured event is triggered. – After configured, LOGO! CIM can perform an action, for example, change the data in UDM, send one or more short messages to one or more contacts. • Mobile cellular With the CIM, you can establish a mobile data connection to a mobile cellular network. • GNSS position – Display the position information on the web page – Enable/disable map the position data to UDM • Time Server – LOGO! CIM can act as an NTP server to provide time for LOGO! BM or other NTP client. – LOGO! CIM can enable/disable mapping the time to the Universal Data Model (UDM). Then the device without NTP can get the time via multi-protocol or RESTful API. • Power on/off SMS – CIM can send a power on/off SMS to one defined contact.
|
This contribution was helpful to
1 thankful Users |
10/1/2021 4:46 AM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33413 Rating:
|
Now there is a delivery release for the LOGO! CIM: The manual can now be downloaded again: LOGO! CIM Edition 10/2021 |
This contribution was helpful to
2 thankful Users |
Follow us on