12/10/2021 8:27 AM | |
Joined: 8/21/2019 Last visit: 12/7/2023 Posts: 13 Rating: (0) |
hi all am using CP 343 - 1 advanced, i already inserted Profinet IO and link with my vision system. i can able to find my vision controller in available devices and i try to flashing from PLC also ok. But when i try to exchange data PLC -> Vision controller & Vision controller -> PLC cannot able to exchange any data. On CPU and CP also No error. is there any setting have to enable ? Please support. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/13/2021 13:12:50New subject after splitting |
|
12/10/2021 9:00 AM | |
Joined: 8/21/2019 Last visit: 12/7/2023 Posts: 13 Rating: (0) |
Hi Thanks for your quick reply i already done all what you mentioned. please see attached image. |
12/10/2021 9:08 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello, Perhaps you can give some information, how you are trying to read the inputs? Best regards, Wizard |
12/10/2021 10:20 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello, When you use CP343-1 as Profinet IO controller, don't you need some communication blocks to access the IO Devices? See the following link: How do you program communication blocks FC11 and FC12 for the PROFINET IO controller? Best regards, Wizard |
This contribution was helpful to2 thankful Users |
Follow us on