7/7/2021 5:55 PM | |
Joined: 10/20/2005 Last visit: 8/26/2025 Posts: 37 Rating:
|
Hi, I'd like to connect an OUC alication and OPC client to to a simulated PLC via PlcSim Advanced. I've problem with the virtual ethernet adapter. I attach a document with screenshot and details. My PC:
My project
First I configure PLCSim advanced in order to work via Softbus connection. Then I’m able to go online, search for nodes and load project to simulated CPU: Now I can go online with TIA project, check DBs and more. Simulation via Softbus is OK. So, Ithink there are not compatibility issues with Windows or PLC model. But, if I set communication via virtual ethernet adapter, I am no longer able to connect to the simulated PLC. No way. Do you have any suggestion? Thanks, Best regards. AttachmentPLcSim-advanced.pdf (736 Downloads) |
8/9/2022 10:03 AM | |
Joined: 5/25/2021 Last visit: 5/29/2025 Posts: 25 Rating:
|
Same here, if I use entherent adapter I can't connect |
Last edited by: AutoGen_1797064 at: 08/09/2022 10:03:52 |
|
Follow us on