4/30/2013 8:02 AM | |
Joined: 10/22/2011 Last visit: 8/26/2024 Posts: 299 Rating: (1) |
Hi I am sending you the project file of TIA V11. Please see the file and tell me if there is any mistak? Waiting for reply. Thanks Attachmenttest.zip (246 Downloads) |
5/14/2013 7:48 PM | |
Joined: 10/22/2011 Last visit: 8/26/2024 Posts: 299 Rating: (1) |
Hi Sir, Thanks for help. Now program is dowloading in the plc without any error. but now problem is that ERROR indication on CPU is continuously blinking. what may be the reason? I am sending you some pics. I am sending you the program, in which I am trying to output a certain V between 0-10V selected by HMI interface. It means that If one HMI is connected to the plc and i enter a decimal value like 300, 400, 420, 430, 470 ..... etc then QW should produce voltage accordingly. waiting for reply. Thanks AttachmentProject1.zip.zip (250 Downloads) |
Follow us on