1/11/2016 9:25 PM | |
Posts: 4 Rating: (0) |
i need to conect a dataman DM260 whith plc 1200. i can´t read the data in the PLC help please |
1/11/2016 11:36 PM | |
Joined: 9/27/2006 Last visit: 11/10/2024 Posts: 12293 Rating: (2691) |
Hello Angel; Searching the Cognex website, it seems that the Datama 200 series is Profinet capable. As you probably know, the S7-1200 has an integrated Profinet port that you could use to connect with the Dataman 260, using the provided GSD file. See the following tutorial from Cognex on Profinet for the Dataman series (there are also 2 articles in the Cognex Knowledgebase on Profinet problems and solutions): https://www.cognex.com/support/downloads/File.aspx?d=2337&langtype=1033 Hope this helps, Daniel Chartier |
1/12/2016 12:51 AM | |
Posts: 4 Rating: (0) |
thanks daniel!!! i finished to install of file GSD and I can to send a trigger (dataman). but I can´t read the date of scanner in the PLC
|
1/12/2016 2:26 AM | |
Joined: 9/27/2006 Last visit: 11/10/2024 Posts: 12293 Rating: (2691) |
Hello Angel; The Cognex site seems a very well organized and instructive place to look for information on the networking of your Dataman 260. You should look at the Profinet section of this document (from page 123):
DataMan Communications and Programming Guide
https://www.cognex.com/support/downloads/ns/5/36/68/CommunicationsAndProgramming_5_6.pdf Look at the attachment for a hint (and an example program from page 141) Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/12/2016 2:39:10 AM |
|
1/13/2016 3:38 PM | |
Posts: 4 Rating: (0) |
thanks!!!! Daniel. Ready I can conect and receive data...Thanks
|
Follow us on