7/6/2009 9:34 AM | |
Joined: 10/7/2005 Last visit: 11/18/2024 Posts: 3027 Rating: (1057) |
Hello KOURTZAAR have a look at this FAQ whichI hope will help. |
Cheers |
|
7/6/2009 10:31 AM | |
Joined: 10/7/2005 Last visit: 11/18/2024 Posts: 3027 Rating: (1057) |
Hello again, it's always reccomended to go for the latest firmware (V5.3 in your case) which you'll find here: Firmware Updates for S7-416-CPUs Please note that it is easy to pick the wrong CPU in the list, make sure to read the part numbers carefully andto download the correct firmware. A firware update will also fully "reset" you CPU to factory default (i.e the online SDB will be gone) HWconfig V5.1 is by the way the one to use for firmware V5.1.0 (Siemens sometimes doesminor firmware upgrades such as V5.1.1 in which case you'll still use V5.1 from the HWconfig catalogue). P.S: Which Step7 version are you using? |
Last edited by: fritz at: 7/6/2009 10:33 AMCheers |
|
7/6/2009 11:18 AM | |
Joined: 10/7/2005 Last visit: 11/18/2024 Posts: 3027 Rating: (1057) |
Have another look at the firmware link that I gave you, as of firmware V5.0 you can also do an online firmware update (no need for a flash Eprom card). |
Cheers |
|
7/6/2009 1:59 PM | |
Posts: 48 Rating: (1) |
Hello mumbles, i find it very useful and i use this in future.Thank you very match. |
Follow us on