6/14/2013 12:28 PM | |
Posts: 3609 Rating: (29) |
Import of a technical question from user valski
|
6/21/2013 10:14 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
hi can you please explain what is your requirement |
Jazz |
|
6/26/2013 5:09 AM | |
Joined: 5/17/2010 Last visit: 2/21/2022 Posts: 80 Rating: (1) |
Hi Valski, Can you upload the program? If the program not processed, have you call the block yet? From the OB1 call the Function Block. |
6/26/2013 5:41 AM | |
Joined: 4/17/2012 Last visit: 8/30/2024 Posts: 474 Rating: (10) |
Hi Valski, in this logic some where you are loading the output value in Temp Variable of FB so each and every cycle it overwrite and made the result zero.
|
6/27/2013 3:42 AM | |
Posts: 15 Rating: (0) |
Hi All, To be clear and precise with my query. I have downloaded the program to my PLC CPU, switch to RUN mode and called the FB. connected the prox sensor to my DI module (this happens to be in the DI-slot 4 with address of I0.0). I simulated via a variable motor with 4 targets/1 rev. to see if the program works. I can only view the (on simulation mode) the bit transition from 1 to 0 during the target that passes on the sensor but could not see any output or speed indication on my program simulation. Could anybody explain thoroughly or correct, edit the program to make itwork, and or any advice if this program will work. Thank you very much |
Follow us on