1/5/2014 11:45 AM | |
Joined: 1/28/2009 Last visit: 1/22/2022 Posts: 21 Rating: (0) |
Dear all please, i have problem with install simatic step 7 v5.5 in win 8 32bit . can any one helpe me |
1/5/2014 3:07 PM | |
Joined: 5/19/2011 Last visit: 4/12/2024 Posts: 24 Rating: (1) |
I don't think Win8 is supported yet. Software requirements STEP 7 version V5.5 is released for the operating systems below:
The STEP 7 software is released for Windows XP Professional (32-bit). Installation in Windows XP Professional X64 (64-bit edition) is not possible. *STEP 7 V5.5+SP1 (or higher) Internet Explorer More information is also available in our FAQ on "Compatibility of STEP 7 versions with the MS Windows operating systems" in Entry ID:8250891. |
This contribution was helpful to1 thankful Users |
Follow us on