9/9/2010 3:02 PM | |
Joined: 1/26/2007 Last visit: 7/29/2025 Posts: 123 Rating:
|
i ask also here , to do not open a new thread. my micromaster is running controled via profibus by an c7 635 . 2 weeks ago , it happend an damage of power connection to the engine . the engine was repaired , and now , al line is runningon a fix speed. when i want to chenge the speed , it shour runn with a very low speed (2 m/s = few rotation). when the speed is going down , the system goes to SF+ BF , and stopp the line . do you have any suggestions where to look into the parameters , and to check ?? Thank you in advance . Splitted from Is it possible to save parameters from Micromaster 440 ??. |
Last edited by: O_Moderator at: 9/13/2010 2:40 PMnew subject after splitting |
|
Follow us on