8/29/2023 10:55 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi hewking103, The PROFINET topology must be configured for device replacement without exchangeable media. The easiest way to do this is to use the topology view and create the port connection there. For more information, refer to the "PROFINET with STEP 7" function manual, chapter "Device Exchange without Exchange Medium". Kind regards |
Follow us on