7/21/2014 10:24 AM | |
Posts: 1368 Rating: (126) |
And another thing to try: can you remove the 1Hz on the REQ and try to call the PUT/GET with only one REQ = true? |
7/21/2014 6:21 PM | |
Posts: 5225 Rating: (1192) |
Thanks to Pittiplatsch for all the help given already. Please jinga may we have a piece of the program as to assist you better. I propose the smaller version you are using to test communications. I am sure with that, my friends will be able to be of more help. PS: That is to say if the problem is software and not hardware or hardware configuration. Regards, w |
6/2/2015 3:57 PM | |
Joined: 9/1/2005 Last visit: 10/4/2024 Posts: 4105 Rating: (195) |
new question published by rstack is split to a seperate thread with the subject put/get not working error 4 appears
Best regards |
My Forum is the place to personalize your profile, |
|
6/13/2016 10:11 AM | |
Posts: 2 Rating: (0) |
Hello Is it Possible to transfer STRING data type via PUT?? |
Follow us on