8/4/2022 9:21 AM | |
Joined: 2/7/2018 Last visit: 3/14/2023 Posts: 181 Rating: (30)
|
Hello, between the S120 and S210 there are several differences: - S120 is a multi-axis system / S210 is a single-axis system - the S210 can only be used with the servomotors simotics 1FK2/1FT2/1FS2 - the S120 can be controlled with EPOS or technology objects / S210 only with technology object - performance between both is comparable Here are two links to the catalogs: - S210: https://support.industry.siemens.com/cs/ww/en/view/109754381 - S120: https://support.industry.siemens.com/cs/ww/en/view/109751875 For detailed information regarding the differences I recommend to get in touch with your local Siemens contact. Best regards TechSupport for SINAMICS S210 |
Follow us on