6/21/2024 9:21 AM | |
Joined: 10/6/2010 Last visit: 7/26/2024 Posts: 14 Rating: (0) |
Hi, I have a scalance S615 that is placed between a DCS and a CP-443-1 I am programming the scalance using the web.management, not by the Tia portal. The DCS have a network address 192.168.121.xx and the CP-4431 have 192.168.101.xx, so I have selected the NAT for link the two different networks. I need to use the protocol ModbusTCP-IP. VLAN 1 and VLAN2 are already created inside the Scalance, so ports 1,2,3,4 are linked to VLAN1 and Port 5 is linked to VLAN2 .. See picture 1 In the NAT area i have selected the NAPT and i had configured two port forwardings form VLAN1 to VLAN2 and viceversa. I am not able to set the STATIC ROUTES funcion, because the scalance doesn't accept the subnet mask 255.255.255.0 I had disabled the firewall. Pinging the addressess for VLAN2 (Port5) to CP-443-1 (VLAN1) doesn't work, and also the Modscan does't work. Someaone had already use this funktion? Thanks AttachmentPICS.zip (24 Downloads) |
6/21/2024 9:50 AM | |
Joined: 2/24/2011 Last visit: 7/29/2024 Posts: 57 Rating: (5) |
Hello, you find information in chapter 5.8 of the manual SIMATIC NET: Industrial Ethernet Security SCALANCE S615 Web Based Management V7.2 and in the FAQ Which NAT scenarios can you realize with SCALANCE SC-600 / M-800 / S615? . Otherwise you should open an own support request. The Customer Support can check your security configuration. |
This contribution was helpful to1 thankful Users |
Follow us on