10/19/2009 2:00 PM | |
Posts: 510 Rating: (117) |
I hope you find this CAD file useful
AttachmentS7-1200 Laser and Wiring Diagrams.zip (28871 Downloads) |
This contribution was helpful to51 thankful Users
|
10/19/2009 7:04 PM | |
Posts: 510 Rating: (117) |
Sorry, Here is a link for a free CAD file viewer from Autodesk. I use it. http://usa.autodesk.com/adsk/servlet/pc/index?id=6703438&siteID=123112 here is another link http://www.infograph.com/products/dwgviewer/ and another http://www.autodwg.com/dwg-viewer/?gclid=CP2R5O_KyZ0CFcQSzAodG3t9uA and a couple more http://www.brothersoft.com/downloads/cad-viewer.html The file is provided for people using the 1200 to easily generate drawings. regards, billwest |
This contribution was helpful to4 thankful Users |
6/18/2010 3:41 AM | |
Posts: 1 Rating: (0) |
For any one that use AutoCAD and work with the S7-1200 series P.L.C. this is excellent, thanks |
8/6/2010 4:37 PM | |
Posts: 4 Rating: (0) |
is there an updated version of this file that has the RTD Modules? |
10/27/2010 11:42 AM | |
Posts: 378 Rating: (47) |
Hello, maybe a little bit late, |
This contribution was helpful to4 thankful Users |
11/21/2011 4:54 PM | |
Posts: 1 Rating: (0) |
Hi Bill, Do you also have this file including the covers of the connections? thanks, Mark |
5/8/2013 7:28 AM | |
Joined: 11/15/2012 Last visit: 4/8/2024 Posts: 9 Rating: (0) |
Usefull for Autocad! Thank you and congrats! |
5/9/2014 8:18 PM | |
Posts: 1 Rating: (0) |
Thank you! |
This contribution was helpful to1 thankful Users |
Follow us on