7/25/2017 7:35 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, HMI Backup you can do with PROSave, this is a non editable Backup which can be used to restore the project to another panel of the Same Type. A Upload/Backup of the HMI to edit the program is not possible, here you need the origin Engineering project which was loaded to the Panel! For PLC you can make a Backup in TIA in the Online Menu, here also a non editable Backup was created for restore to another PLC with the same Type. For PLC exist this FAQ which describe which Upload/Backup is possible: https://support.industry.siemens.com/cs/ww/en/view/9755405 Christoph |
7/25/2017 7:36 AM | |
Joined: 12/16/2012 Last visit: 4/24/2024 Posts: 652 Rating: (130) |
Hi! You can backup or restore your HMI with e.g. ProSave or a memory card. However, you will not be able to edit the backed-up file since it is not the full TIA HMI project, but a generated/compiled file (except for WinCE panels). how-do-you-back-transfer-the-projects-of-an-operator-panel-and-what-should-you-watch-out-for |
Follow us on