3/19/2015 9:47 PM | |
Joined: 11/29/2011 Last visit: 10/24/2024 Posts: 1360 Rating: (232) |
Hi, Regarding to your first question: Open theSIMATIC Industrial Software SIMATIC Safety - Configuring and Programming manual under chapter "2.1 Overview of Configuration" where you can read: "Which F-components can you configure with the STEP 7 Safety Basic V13 SP1 optional package? I hope I could help a bit. |
- What you read here, please check with manuals and your requirements. |
|
3/19/2015 11:41 PM | |
Joined: 11/29/2011 Last visit: 10/24/2024 Posts: 1360 Rating: (232) |
Hi, Try this link Failsafe Modules
|
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
3/26/2015 1:21 AM | |
Posts: 73 Rating: (20) |
Hi, For S7-1200F you need to install Step7 V13 SP1 Professional and Safety Advanced V13 SP1. Both of these may be downloaded from the customer support as trial license. This will add the S7-1200F CPU to the hardware library and will allow you to create a safety program. For the failsafe IO you must install the HSP pack for TIA Portal found here https://support.industry.siemens.com/cs/us/en/view/72341852 Once this is done you will see the S7-1200F and S71200F-SM's If you are using Step7 V13 SP1 Basic then you will need to use Safety Basic V13 SP1. In this case it must be ordered. Or perhaps Siemens will provide a trial download for this as well, I guess we will see when they post the info. Goodluck |
6/6/2018 2:53 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by kaankirmc is split to a separate thread with the subject Safety I-device communication between 2 PLC. Best regards |
Follow us on