7/11/2009 10:54 AM | |
Posts: 34 Rating: (0) |
Only some OPs are supported, not even runtime scada ... But after two years, they might combine them wincc scada basic with wincc |
8/6/2009 1:29 PM | |
Posts: 76 Rating: (1) |
why do you think that it will be after 2 years? We wish it in 1 year! |
9/1/2009 12:28 PM | |
Joined: 9/23/2005 Last visit: 11/4/2024 Posts: 4351 Rating: (1452)
|
Hi, Take a look at the FAQ “How do you access tags of S7-1200 with a panel or RT configured with WinCC flexible 2008 SP1?” http://support.automation.siemens.com/BR/view/en/38112005. Despite of the “system test” comes only with WinCC flexible 2008 SP2, there is there a step by step of the communication setup. Note: in the FAQ is used Rack 0 and slot 1. |
Denilson Pegaia |
|
9/1/2009 1:41 PM | |
Joined: 5/28/2008 Last visit: 10/23/2024 Posts: 1343 Rating: (141) |
Hi, the link doesn't work. And what about WinCC flex 2008 SP2? regards Robster |
9/8/2009 12:55 PM | |
Joined: 9/23/2005 Last visit: 11/4/2024 Posts: 4351 Rating: (1452)
|
Hi, an version of the above mentioned FAQ now is released for Internet: http://support.automation.siemens.com/BR/view/en/38112005 |
Denilson Pegaia |
|
9/8/2009 1:54 PM | |
Joined: 5/28/2008 Last visit: 10/23/2024 Posts: 1343 Rating: (141) |
Sorry, but it is the same link like above |
Follow us on