12/21/2021 4:25 PM | |
Joined: 12/21/2021 Last visit: 12/23/2021 Posts: 7 Rating:
|
Hello, I'm relatively new to Siemens but I have put together 5 or so machines using this same rack configuration. My second card in the rack is an F-DI 16VDC and it is coming up as not reachable. It is strange because I swapped the card out for another identical card and it worked but over night it started flashing red again by the time I got in in the morning. Both cards now boot up flashing red. I have verified the supply voltages and currently this card is running on it's own dedicated power supply. I have all other wires to the card removed only L+, M, and ground are connected. PLC - CPU 1215FC DC/DC/DC - 6ES7 215-1AF40-0XB0 F-DI - SM 1226 F-DI8/16 x 24VDC - 6ES7 226-6BA32-0XB0 The part numbers all match what is printed on the cards. Anyone have any ideas? AttachmentDiagnostics.txt (458 Downloads) |
Last edited by: WldEng at: 12/21/2021 16:38:29 |
|
12/21/2021 4:27 PM | |
Joined: 12/21/2021 Last visit: 12/23/2021 Posts: 7 Rating:
|
Here is a picture of my device overview. |
12/23/2021 3:28 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, If you are not sure what I mean, you should have a look into the safety manual: Assigning a PROFIsafe address of the F-I/Os with SIMATIC Safety this is an essential step when projecting F-modules. regards, |
FCK WAR! |
|
12/23/2021 3:46 PM | |
Joined: 12/21/2021 Last visit: 12/23/2021 Posts: 7 Rating:
|
I did some research and I don't have an assign profisafe address button. Is assigning profisafe addresses automatic with the 1200 or with TIA v16?
|
12/23/2021 3:51 PM | ||
Joined: 12/21/2021 Last visit: 12/23/2021 Posts: 7 Rating:
|
From your link.
|
|
Follow us on