11/17/2008 10:51 AM | |
Joined: 11/17/2008 Last visit: 2/12/2020 Posts: 3 Rating: (0) |
Is it possible to use Wonderware Intouch (Version 9.5) with S7-PLCSIM (Version 5.4 + SP1) using the Ethernet connection setting via a DASSIDirect IO Server (Version 1.0 SP1 Patch 1)? Please could anyone help if they have any info - this system is working ok on site withthe PLC hardware but I would like to settup the system in the office with a S7-PLCSIM. Further info below on the configuration: I have a Virtual machine running with a Step7 program downloaded into S7-PLCSIM (Version 5.4 + SP1) using the Ethernet connection setting (IP address 192.168.0.1). The Simatic Manager PG/PC Interface is set to PLCSIM(RFC 1006). The S7-PLCSIM is running and blocks are available to view online. Wonderware Intouch installed (Version 9.5). Access Names have been created with application name set to DASSIDirect, protocol = suitelink and advise all items. The System management console DAServer DASSIDirect Configuration (Version 1.0 SP1 Patch 1) has been set up with the IP address of the PLC, Local TSAP = 1,0 and Remote TSAP = 0,3,3 and device groups have been created matching those settup in the Intouch config.
AttachmentIntouch PLCSIM Query.zip (864 Downloads) |
10/10/2009 9:48 AM | |
Posts: 45 Rating: (8) |
Hi everybody, Maybe, PLCSIM OPC Server may help? |
Last edited by: SSE at: 11/2/2009 10:49 AM |
|
Follow us on