5/18/2012 9:34 AM | |
Posts: 6 Rating: (0) |
Hi Ganes10 In CPU It is clear to me. I have problem with define Tag in panel KTP 300 for backlight color |
5/18/2012 11:02 AM | |
Joined: 8/31/2010 Last visit: 9/3/2024 Posts: 1520 Rating: (227) |
Hello popi, Did you try this in KP300 as shown in the enclosed screenshot? Still not working? |
Like it? Rate it! |
|
5/18/2012 12:59 PM | |
Posts: 6 Rating: (0) |
Yes It works |
This contribution was helpful to1 thankful Users |
6/22/2012 8:41 AM | |
Joined: 12/5/2007 Last visit: 9/12/2024 Posts: 1 Rating: (1) |
HI Guy's Much simpler way of changing colour , using one tag only, and changing value from 0-1-2-3 to change background screen colour 95% done using an event change from the HMI tag attribute on the HMI, only 1 tag from PLC Portal sample project attached Stu.. Attachmentktp300 background colour change portal sample V11sp2.zip (750 Downloads) |
Follow us on