4/13/2008 4:06 PM | |
Posts: 27 Rating: (0) |
hi! I constructed the Ring network with two IRT by using 11 X208. The role of two IRT is Redundancy Manager and edundancy Client. This Ring network was normal for several months. One X208 was downed several days ago. Failure diagnosis LED of X208 had been turned off. And, I was not able to log in this x208. And, PST cannot discover this X208. The transmission rate was 10Mbps though I connected PC directly with this X208.10Mbps is abnormal. I think that 100Mbps of the transmission rate is normal. Four X208 was this time downed several days later. Four X208 seceded this time from the network several days later. I was able to use PST and I.E by connecting PC directly with one of these four HUB. And, the other three X208 was able also to log it in with I.E. The Ring wiring uses all Port1 and 2. And, Port1 and 2 of all HUB are green LED. In a word, physical wiring of all Port1 and Port2 exists. Green LED has blinked to RM of IRT now. There was no error packet though I confirmed Packet of all HUB. There seem to be two troubles in this Ring network. One is a down of one X208. Another is an imperfect Ring network. To solve the first trouble, I installed new X208. However, this trouble cannot be solved. PST cannot discover this X208.The content of the trouble is quite the same. Why cannot the trouble be solved? I do not understand the second trouble. Why have four HUB seceded from other HUB to the existence of the Ring wiring? Someone, please let me knowt the method of settlement. Thanks, 931221 Attachmentnetwork.pdf (545 Downloads) |
4/14/2008 8:03 AM | |
Posts: 27 Rating: (0) |
HI! >What do you mean by HUB in this sentence? Do you mean switch? And is it integrated in the >Host PC of is it a special NIC which uses the Teaming I mentioned?
HOST PC and HUB of Cisco are special specifications. There is one kind of IP of HOST PC. However, there are two NIC. >Could it be that there are some nodes connected to the network which are not able to do Auto >Negotiating? In Port3(cisco) of two IRT, status of 100M FD and Negotiation is disable. Perhaps, the auto negotiation function is Disable in Cisco. >Maybe then the X208 are not able to switch over to the right mode. >If this is not possible lots of collisions can occur which makes the switch a little bit slower. Is it AP504?Or, is other X208? I do not understand the reason why AP504 doesn't operate at all. Diagnosis LED of AP504 is not red. Thanks, 931221 AttachmentNETWORK.zip (472 Downloads) |
Last edited by: 931221 at: 4/14/2008 10:23 AMLast edited by: 931221 at: 4/14/2008 8:47 AM |
|
Follow us on