9/29/2016 12:50 PM | |
Joined: 5/12/2006 Last visit: 11/12/2024 Posts: 22446 Rating: (3029)
|
Hi, you should have a look on the PNIODIAG Application example. https://support.industry.siemens.com/cs/ww/en/view/98278878 i think it is exactly what you need.
Christoph |
9/29/2016 1:22 PM | |
Joined: 2/27/2014 Last visit: 9/4/2024 Posts: 689 Rating: (200) |
Hello, Always define the statement of your problem in detailed way. Important to know, are you going to use new HMI as comfort series or you want to integrate with old series HMI? For existing HMI/WinCC flexible, the link which Christoph has given is exactly true. But if you are going to show with new series HMI under TIA portal then you need to migrate wincc flex project to TIA with available link. https://support.industry.siemens.com/cs/ww/en/view/98278878 You need to use FB126 at PLC side in program. For TIA portal application plz find the attached application. If you feel this post is useful then don't forget to rate AttachmentPNIO-Diag1_82.zip (382 Downloads) |
Last edited by: DJ_1 at: 9/29/2016 1:24:46 PMWith Best Regards, |
|
This contribution was helpful to1 thankful Users |
10/1/2016 1:38 PM | |
Joined: 9/2/2012 Last visit: 8/15/2024 Posts: 711 Rating: (30) |
Dear DJ, thank you for sharing the details. May i know from where you got this library? I was searching for this for quite long time, but not succeeded. 1.The program attached by you is for PLC and HMI in TIA platform, right ? 2. Do you have PLC,HMI project together ? 3. I have added s7-300 in the same pjct and activated diagnostics as shown in attachment. But how DB126 is getting generated ? If possible, kindly share the FAQ. If not available step by procedure will be helpful.. AttachmentPNIO.zip (210 Downloads) |
|
|
Follow us on