12/7/2017 12:54 AM | |
Posts: 1283 Rating: (105) |
Hi All, I am now working with SIEMENS LOGO OBA8 and just wanna know some details regarding VM Mapping. 1.If I am not connected to the LOGO, can I do the VM Mapping Offline? 2.Is there any restriction for Mapping offline? Because I had seen only the variables which are not physically wired is been displayed offline, say for example Analog comparators and stuffs like that. Any help on this is highly appreciated.. Thanks, Prasanth ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/7/2017 7:39:32 AMNew subject after splitting |
|
12/7/2017 9:45 PM | |
Joined: 2/12/2016 Last visit: 1/8/2024 Posts: 69 Rating: (9) |
VM maping for 0BA8 see pdf FrantaM AttachmentLOGO!%200BA8%20Reserved%20VM%20addresses.pdf (4032 Downloads) |
This contribution was helpful to7 thankful Users |
9/24/2020 7:18 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
V0.0 - V0.7 = VB0 V0.0 - V1.7 = VB0 + VB1 = VW0 V0.0 - V3.7 = VB0 + VB1 + VB2 + VB3 = VW0 + VW2 = VD0 The addressing is byte-oriented. With a word (VW) or double word (VD), the address (e.g. VD4) is the specification of the first byte (with VD4 it is VB4). The address of a V bit (Vx.y) is made up of the byte address x and the bit address y. V0.4 = bit 4 in byte 0.
AttachmentLOGO! Bit, Byte, Word and DWord.pdf (1940 Downloads) |
Last edited by: ixo65 at: 09/24/2020 21:29:56 |
|
This contribution was helpful to6 thankful Users |
Follow us on