5/24/2023 6:35 AM | |
Joined: 5/23/2023 Last visit: 5/3/2024 Posts: 3 Rating: (0) |
GoodMorning! I am looking for the SIMATIC S7-Fail-safe Configuration Tool (S7-FCT) but i can't find the download. I could only find the download of SIMATIC_S7_FCT_V3_UPDATE1 but after the installation i can't find any application to run, maybe that is just an update. Maybe there is no compatibility between my windows version and the S7-FCT, i have Windows 10 Enterprise 21H2. Thanks. Best regards Damiano |
Last edited by: AutoGen_2970859 at: 05/24/2023 07:28:18 |
|
5/24/2023 8:58 AM | |
Joined: 5/6/2022 Last visit: 5/6/2024 Posts: 416 Rating: (82) |
Hi AutoGen_2970859, I imagine that the file that you have downloaded, you have done it from this FAQ that I share below, right? SIMATIC S7-Fail-safe Configuration Tool (S7-FCT) It is the only thing that I have been able to find and according to what is said it seems that it is the software and it does not show the update, maybe I am wrong. Therefore, after looking in the SIMATIC Industrial Software SIMATIC S7-FCT V3.0 - Fail-safe Configuration Tool manual, I have seen that the OS you mention is missing. Therefore, it makes me suspect that they are possibly compatibility issues. I am going to check if I also find the compatibilities in the siemens compatibility tool and I will update the post. Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on