11/9/2013 11:16 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
Hello, the SIMOTION Firmware you can Download here. Delete the existing MMC card an extract th downloaded FW into the Root of the MMC. Then put the MMC in the C230-2 and the Downgrad begining. After the Downgrade you can go online with your V3.2 Scout/Project. The Version in the Module means in stored FW Version in the C230.2. To check the FW with Scout you must use a Scout which support the FW Vesion. If you have a C230.2 V4.1 you need a Scout V4.1 because the Scout V3.2 don't know the C230.2 V4.1. Regards Christoph |
Follow us on