11/13/2008 1:57 PM | |
Posts: 56 Rating: (0) |
All, Can i UPLOAD from Simotion C230-2 CPU without original programme backup?. Is it possible to take a backup of Original CPU from Memory card?. Regards, Anguraj |
11/14/2008 9:02 AM | |
Posts: 116 Rating: (7) |
Hi, have a look to the new SIMOTION V4.1 SP2-Functions --> see: http://support.automation.siemens.com/WW/view/en/32113692 Download the PDF "Simotion_New_Functions_V412.pdf" See Chapter 3.1: Load project from the device „Upload in case of missing or not current project“ This yould be a possibility for you. Regards Jerry |
11/19/2008 10:01 AM | |
Joined: 9/24/2008 Last visit: 10/2/2024 Posts: 30 Rating: (8) |
If you are using v4.1 SP2 you can upload the HWConfig as well as the programs and technology objects. See attched extract from the manual. There are a couple of points to note: AttachmentLoadToPG.pdf (446 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on